Homeowner Tips

Survey Shows Comfort is the Hidden Hero at Holiday Gatherings


comfort is the hidden hero

Our latest survey shows temperature plays a critical role in maintaining high spirits during holiday gatherings. From prepping the perfect playlist to cooking a delicious meal, a lot of preparation and detail goes into planning a holiday get-together and making sure your guests have a good time. Unfortunately, all that hard work can be undone by something as simple as the temperature in your home.


According to our survey, 50% of people would leave a party early if they didn’t feel comfortable with the temperature at the gathering.


When it comes to surprising statistics from this survey, we’re just warming up. While a home-cooked feast may seem like the most important part of a holiday celebration, the temperature holds just as much significance. In fact, more people would rather fake their enjoyment of the food or stay hungry than be too hot or too cold inside.

And, while  spending hours adorning your home with seasonal décor may be a tradition, make sure not to overlook the impact temperature can play in your home during the holidays. Our survey found, nearly one-third said the temperature can make them feel just as festive as the decorations.


While 88% of Americans think it’s rude to change someone else’s thermostat, over half of respondents said they have or  they know someone has changed a family member’s thermostat during the holidays without telling them.

The good news is we have insight into the ideal temperature for all of your holiday hosting. Most survey respondents reported preferring similar indoor temperatures, with the ideal temperature hovering around 70 degrees. In fact, 66% of those surveyed say their ideal indoor temperature falls between 68 and 72 degrees.


This holiday season, a Sensi Smart Thermostat can solve all of your home comfort woes. With its flexible features and integrated technology, the Sensi smart thermostat creates the ideal setting for every season by putting control and ease at users’ fingertips – ensuring your holiday season can be a success.


But don’t just take our word for it – see why Travel+Leisure featured Sensi thermostat in their cool gadgets. Named the 'Best Overall' Smart Thermostat and 'Best Value' Smart Thermostat for three straight years by USA Today’s Reviewed.com, Sensi Smart thermostats have been recognized for their excellence time and again.


You can purchase a Sensi from many contractors and retailers – and because of holiday season sales, this is the perfect time to treat yourself. Check with Best Buy, Home Depot, Lowe’s or Amazon to find the deal that’s right for you, and then find a pro to install it!


Home comfort during the holidays starts with Sensi.

Please enable JavaScript to use this website.