Features & Controls

Learn about your Sensi thermostat app

Take advantage of these Sensi thermostat app features


One of the best features of owning a Wi-Fi thermostat is the ability to have complete control of your home comfort, from across the couch or across the country. The Sensi™ Smart Thermostat app serves as your personal remote control, providing instant access to your thermostat via your smartphone. Change system settings, adjust the temperature and set or change schedules when you’re on the go - or just don’t want to get up.


We are continually making improvements and feature updates to the Sensi thermostat app to be intuitive and more useful to you, so here are some key features new and old.


In-app Usage Reports

No more waiting for monthly summaries — now, you can monitor current day and historical heating, cooling and fan runtimes right in the app

Dashboard

The app is now easier to navigate through multiple thermostats thanks to a dashboard view - from one thermostat to many, you can control your comfort with a few taps. To access more detailed information about a thermostat, tap on the thermostat name and be taken to the thermostat detail view.


Geofencing

For those living an unprogrammed life, we created the Geofencing feature. By using your phone’s location relative to your individual thermostat’s location, we can automatically set your mode to home or away, creating a 3-degree offset to save you money while you’re gone. You will need to enable the geofencing feature for each thermostat in your home.


Read more about using the Geofencing feature.

           

Program a Schedule
The Sensi thermostat app lets you create custom temperature schedules for each day of the week (up to seven independent schedules). This makes it easy to create one or multiple schedules to match your family’s routine. Using the Sensi thermostat app, select the days you want to follow a specific schedule. Then choose the time and temperature set points for each. When you are running a schedule, scroll across the Thermostat Detail View on the home screen to see your scheduled temperatures for the next 24 hours. You can also press on any of the temperature bubbles to open that specific schedule and make changes. Read more about Sensi thermostat schedules and settings.


If you or someone in your family makes an adjustment to the temperature at the actual wall unit while you are running a schedule, this will activate a temporary temperature change that lasts for 2 hours. This temporary change is displayed in the thermostat app by a white bar along the Timeline. This visual tells you the exact time that the change was made and when your original schedule will resume.  

           


Keypad Lockout

Tired of people messing with the thermostat? Enable Keypad Lockout right from the Sensi thermostat app. It’s an easy, convenient way to prevent accidental (or intentional) setting changes to your thermostat. It locks the buttons on the actual wall unit, but you maintain full control from your mobile app. Find the Keypad Lockout feature in your Advanced Settings. Learn more about Keypad Lockout.  


Set Point Controls

If you are using the Auto Changeover (“Auto”) system mode, you can keep your home temperature within a specific range. Press and hold the set point buttons to make them move faster.

Temperature Offset
If you have just installed a new Sensi thermostat, you might be used to the readings on your old unit. Temperature Offset is a feature that lets you adjust the room temperature reading +/- 5°F to match your preference. This is also useful if your thermostat is located in a particular warm or drafty location and isn’t an accurate reflection of your room temperature.


(It also comes in handy if you want your spouse to think it’s a particular temperature so he/she won’t keep adjusting the thermostat. For this instance, we suggest using this feature wisely.)


System requirements:
iOS - 15.0 or above
Android - 8.0 or above

           


Thermostat Detail View

After observing how users interact with our iOS and Android applications, we made usability enhancements to surface the most commonly-used features on the thermostat. We removed the side menu and replaced it with a tab bar on the bottom of the thermostat detail view. You can now access thermostat settings and scheduling quickly and easily.


Circulating Fan

The circulating fan feature allows the fan to circulate air when the system is not running. A percentage is selected to indicate how often the fan should run each hour. Simply tap the Fan Mode icon on the app and toggle circulating Fan On. Then you can set the percentage you’d like the fan to run each hour. Learn more about circulating fan.


HVAC Service and Filter Reminders 

No more forgetting to change your furnace filter or schedule HVAC maintenance. In-app service reminders from Sensi make it easier than ever to keep your heating and cooling system functioning at its peak performance. Set alerts to receive notifications when routine maintenance needs to be done and opt in to receive emails and notifications from your smart thermostat. Set your personalized reminders now.

Please enable JavaScript to use this website.