Installation
How to register Sensi Thermostats
If you want to use the thermostat remotely through the Sensi app, you will need a dedicated Wi-Fi network at the residence to connect and register it.
The only way to register your Sensi thermostat is through the Sensi app installation process. Once you’ve connected and registered the thermostat to your account, you will then be able to operate it through the Sensi app. However, you can always operate the thermostat from the wall unit, and that does not require Wi-Fi.