Installation 

How do I configure my thermostat?


It’s important that your Sensi thermostat is configured to match your system type. If not, then it may not operate your system as expected. You may be unable to switch to Heat Mode or Cool Mode using your thermostat or in the Sensi app.

To update these HVAC settings, you’ll need to be in front of the thermostat.

You can configure the thermostat through the Sensi app or, if you’re a professional, you can access the HVAC settings directly from the thermostat screen.

Using the Sensi App

  • Open the Sensi app.
  • Tap the + sign.
  • Tap your Sensi product.
  • Tap New Installation.
  • Tap Is Currently Mounted.
  • Follow the in-app instructions to remove the thermostat cover, enter the wires you have installed, select your heating system, and reconnect to Wi-Fi. By following these instructions, the app will setup your thermostat according to the wires you have installed and your system type.


Accessing the HVAC settings directly at the thermostat

Find your Sensi model below to find the right instructions.

Sensi smart thermostat


  • At the thermostat, press Menu.
  • Press Next.
  • At Temperature Scale (°F/°C) settings, press Next.
  • Outdoor settings
    • If you have a heat pump, use up arrow button to set this to “HP1”. 
    • If you have an air conditioning unit, set this to "AC1”. 
    • If you have more than one stage cooling, change this to “HP2” or “AC2” to represent this. (You should have a wire in “Y2” if you have more than one stage.)
    • If there is no wire in the "Y" terminal, use the up arrow to change this to "AC0 "to represent no cooling.
  • Press Next.
  • Indoor settings.
    • If you have a gas furnace, oil burner, or boiler system, use the up arrow button to set this to "6A1”.  
    • If you have an electric furnace, set this to "EL1".  
    • If you have more than one stage heating, change this to "6A2" or "EL2” to represent this. (You should have a wire in “W2” if you have more than one stage.)
    • If you have no wire in "W/E", use the up arrow to change this to "FAN "to represent no indoor heating system.
  • Press Next.
  • Reversing Valve Settings. This setting is important if you have a heat pump. Leave the default setting to “o”. If you have a heat pump, and you notice that your system is cooling in Heat Mode, and heating in Cool Mode, change from the default setting to “b”.
  • Press Exit.

Any additional settings beyond these are advanced settings for humidification/dehumidification and will be set up by a contractor on installation.

Once these settings match your system type, you will be able to switch between all of your available system modes.

Sensi Touch smart thermostat


  • At the thermostat, tap Menu.
  • Tap Advanced Set Up.
  • Tap Set Up HVAC Equipment.
  • Tap Change Settings.
  • Outdoor equipment.
    • If you have a heat pump, tap “HP1”. 
    • If you have an air conditioning unit, tap "AC1.”
    • If you have more than one stage cooling, tap “HP2” or “AC2” to represent this. (You should have a wire in “Y2” if you have more than one stage.)
    • If you do not have a wire in the "Y" terminal, tap "AC0" to represent no cooling.
  • Indoor equipment.
    • If you have a gas furnace, oil burner, or boiler system, tap "GA1.” 
    • If you have an electric furnace, tap "EL1." 
    • If you have more than one stage heating, tap "GA2" or "EL2” to represent this. (You should have a wire in “W2” if you have more than one stage.)
    • If you do not have a wire in the "W/E" terminal, tap "FAN" to represent no indoor heating system.
  • Reversing valve position. This setting is important if you have a heat pump. Leave the default setting to “o.” If you have a heat pump, and you notice that your system is cooling in Heat Mode, and heating in Cool Mode, change from the default setting to “b”.
  • Tap Save.

Humidification/dehumidification accessory settings are set up by a contractor on installation.

Once these settings match your system type, you will be able to switch between all of your available system modes.

Sensi Touch 2 smart thermostat


  • At the thermostat, tap the Menu icon.
  • Tap Advanced Set Up.
  • Tap Set Up HVAC Equipment.
  • Tap Configure
    • Outdoor equipment
      • If you have a heat pump, tap “HP1”. 
      • If you have an air conditioning unit, tap "AC1.”
      • If you have more than one stage cooling, tap “HP2” or “AC2” to represent this. (You should have a wire in “Y2” if you have more than one stage.)
      • If you do not have a wire in the "Y" terminal, tap "AC0" to represent no cooling.
    • Indoor equipment
      • If you have a gas furnace, oil burner, or boiler system, tap "GA1.” 
      • If you have an electric furnace, tap "EL1." 
      • If you have more than one stage heating, tap "GA2" or "EL2” to represent this. (You should have a wire in “W2” if you have more than one stage.)
      • If you do not have a wire in the "W/E" terminal, tap "FAN" to represent no indoor heating system.
    • Reversing valve position
      • This setting is important if you have a heat pump. Leave the default setting to “o.” If you have a heat pump, and you notice that your system is cooling in Heat Mode, and heating in Cool Mode, change from the default setting to “b”.
  • Tap Save.


Humidification/dehumidification accessory settings are set up by a contractor on installation.

Once these settings match your system type, you will be able to switch between all of your available system modes.


Sensi Lite smart thermostat


  • Access the settings by pressing and holding the menu icon for 8 seconds or until you see “Setup Outdoor.”
  • Outdoor settings: At the top of the thermostat screen, you will see “Setup Outdoor.”
    • If you have a conventional air conditioner system, use the up/down arrows to set this to “AC.”
    • If you have a heat pump, use the up/down arrows to set this to “HP.”
    • If you do not have a cooling system (no wire in “Y” terminal), use the up/down arrows to set this to “--.”
  • Tap the menu icon once to move to next screen.
  • Indoor settings: At the top of the thermostat screen, you will see “Setup Indoor.”
    • If you have a gas/oil/propane furnace or a boiler, use the up/down arrows to set this to “GA.”
    • If you have an electric furnace, use the up/down arrows to set this to “EL.”
    • If you do not have an indoor heating system (no wire in W/E terminal), use the up/down arrows to set this to “FAN.”
  • Tap the menu icon once to move to the next screen.
  • Reversing Valve or Multi-Stage settings: At the top of the thermostat screen, you will see “Setup.”
    • This screen configures the “OB/*” terminal. If you don’t have a wire in the “OB/*” terminal, then don’t worry about this setting.
    • If you chose “HP” as the Outdoor setting, then you can set this to either O or B using the up/down arrows.
    • If you chose “AC” as the Outdoor setting, then you can set this to 2H or 2C if you have multi-stage heating or cooling, 6 if you have a zone valve, or if you do not have any wire in OB/*.
  • To exit this menu, tap the menu icon until you get back to the system mode change screen.


Reach out to us

Our customer support is available 7 days a week.

Read More...
Click to continue reading
Please enable JavaScript to use this website.