Features & Controls
There are many reasons why people consider purchasing a Wi-Fi or smart thermostat. Some want energy efficiency and need a smart way to go green to help the environment without sacrificing comfort. Others might live in areas where the temperature fluctuates greatly throughout the day. And with such unpredictable weather that they would like to adjust their home temperature from the office so they don’t have to walk into a stifling hot house at the end of a hard day. Business travelers and property managers want to reduce energy waste on an empty house or vacant property. Because they need to lower bills and extend the life of their heating and cooling systems. What do all of these people have in common? The need for improved control of their thermostat.
When considering a smart thermostat upgrade, it’s important to make sure that it provides the right mix of features for you. Some thermostats try to take this control from you by claiming to learn your habits. Are you really that predictable? We don’t think so. Your schedule is varied. You are always on the go. Things change at the last minute. If you’ve had to work late for a solid week, you shouldn’t have to suffer a hot, humid house because your thermostat “learned” that you wouldn’t be home at that time. It’s time to take back control of your home comfort.
Sensi™ Smart Thermostats give you complete control of your home comfort from anywhere, anytime, using Wi-Fi and smart thermostat technology. The Sensi mobile app gives you instant access to your thermostat via your smartphone. It lets you adjust the temperature, change system settings, or set and change schedules for each day of the week. When heating or cooling your home, the screen changes colors – red for heat, blue for cool, and grey when the system is off – so you instantly know which system is currently in use. But that’s not all. There are several smart, advanced features to provide even greater control of your HVAC system.
For example, you can program set schedules and enable Keypad Lockout to prevent accidental setting changes. Or use the geofencing feature. By using your phone’s location relative to your individual thermostat’s location, we can automatically set your mode to home or away, creating a 3-degree setback to save you money while you’re gone.
In the Thermostat Detail View you can see all of your scheduled temperature settings for the next 24 hours.
Next, you can adjust Fan Settings and also use the Temperature Set Point and Controlsto keep your home temperature within a specific range.
Local Weather conditions are tracked by your zip code and your indoor Humidityreadings are conveniently located right at the top of the screen. Use these to decide if you need to adjust your schedules or if you should remember to take your umbrella with you on the way home.
In addition to the smart features on the mobile app home screen, your Sensi thermostat detects and alerts you of any potential problems with your system. This includes everything from humidity alerts to High/Low temperature warnings, so your system runs efficiently.
If you already have a Sensi thermostat, be sure to check out these great features. And if you are considering adding a smart thermostat to your home, choose a Sensi thermostat and let our technology help you to get smart about your home comfort.
Learn more about the Sensi mobile app and using settings and schedules.